Is there a schematic available for the LS1024A-RDB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a schematic available for the LS1024A-RDB?

1,121件の閲覧回数
petecarpani
Contributor I

I'm trying to put the LS1024ASE7MLA and the MC34VR500V6ES in a product that is moving forward and I'd like to see something to verify that I'm making all of the required connections correctly.  I can't seem to find a schematic for the eval board anywhere else.

0 件の賞賛
返信
1 返信

1,036件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Unfortunately the LS1024ARDB schematic is not public. I have seen the LS1024ARDB rev.B schematics. It does not use the MC34VR500V6ES. There are "QorIQ LS1024A Family Design Checklist" and "Multi-output DC/DC regulator for QorIQ LS1/T1 family of communications processors" data sheet on the nxp site. Perhaps you have used these documents already. It can be used to verify your design.

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信