In LS1043A, Debug Console Port Using UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

In LS1043A, Debug Console Port Using UART

1,652 次查看
logeshs
Contributor II

Hi,

We have connected UART1 to Data Switch (Trident 2+). Shall we use UART2 as Debug console port in LS1043A? Please confirm.

Thanks

0 项奖励
回复
2 回复数

1,481 次查看
alexander_yakov
NXP Employee
NXP Employee

From the hardware point of view, LS1046A does not need console debug port, debugging is performed via special debigging connector. If you mean console output of particular software, for example U-boot, than this software can be configured as you wish.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,481 次查看
logeshs
Contributor II

Thanks for your clarification.

We are just looking for optional console output. 

Thanks.

0 项奖励
回复