How to use external interrupt for P2020

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use external interrupt for P2020

1,416件の閲覧回数
mikexiao
Contributor I

In P2020 datasheet, external IRQ is multiplexed with PCI IRQ. How does software configure it so that it can be used as PCI IRQ or external IRQ?

タグ(2)
0 件の賞賛
返信
1 返信

1,058件の閲覧回数
ufedor
NXP Employee
NXP Employee

To configure the signals as PCI INTx it is needed to refer to the following documents:

1) Linux Documentation "Generic PCI Host Controller":

sdk/linux.git - Freescale PowerPC Linux Tree 

2) "Open Firmware Recommended Practice: Interrupt Mapping":

http://www.firmware.org/1275/practice/imap/imap0_9d.pdf 

3) P2020 interrupt mapping DTS from the Linux SDK:

sdk/linux.git - Freescale PowerPC Linux Tree 

To configure the signals as IRQn it is needed to refer to the AN5121 - Introduction to Device Trees, 5 Interrupts:

http://cache.nxp.com/assets/documents/data/en/application-notes/AN5125.pdf 

0 件の賞賛
返信