LS1012 custom board, UART not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1012 custom board, UART not working

2,136 次查看
nattapongsungch
Contributor III

Hello , 

I'm working on LS1012 custom board reference designed from FRDM-LS1012A.

I already programming RCW , U-Boot , PPA and Kernel ITB and try to boot up. But I cannot see console output.

The difference from FRDM-LS1012A is changing OpenSDA chip to FT230XQ-R but still used same port/pin as reference.

Thanks,

Nattapong

标记 (2)
2 回复数

1,800 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Nattapong,

Please create a "Hello World" C bareboard project in CodeWarrior for ARMv8 IDE, and debug this program step by step to check whether "Hello World" could be printed out through UART.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,800 次查看
nattapongsungch
Contributor III

Thank you , Yiping

Right now, i can boot up board and see serial output already.

0 项奖励
回复