How to connect ls2088a using Console Cable DB9 to RJ45

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect ls2088a using Console Cable DB9 to RJ45

3,520 Views
karthimohanraj_
Contributor I

I have to boot the LS2088A-RDB and i have a  DB9 to RJ45 cable. Will this be helpful in connecting since i don't have Codewarrior connector Or please suggest me any other way to connect to this Board other than CW.  

I have some queries regarding the LS2088A: 

1.  Does this board comes with all pre-installed BSP and SDK? so just connecting using DB9 cable should work out of the box? 

2. Is there any prerequisite settings and changes we should do in the LS2088A to use in the First boot.

Thanks,
karthi 

0 Kudos
Reply
5 Replies

3,369 Views
karthimohanraj_
Contributor I

Hi ufedor, 

I have tired connect with pci serial port adaptor(link) and DB9 to RJ45. But i'm not able to connect to Serial console, to check whether the LS2088A is booting or not. 

Can you point me to some connector available which works with LS2088A?

Thanks,
Karthi 

0 Kudos
Reply

3,369 Views
ufedor
NXP Employee
NXP Employee

Personally I'm using Prolific USB-to-Serial Comm Port.


Where did you get the DB9 to RJ45 cable?

The LS2088ARDB has standard DB9 connectors - no need in such cable:

2018-10-18_234450.jpg

0 Kudos
Reply

3,369 Views
karthimohanraj_
Contributor I

Hi Ufedor, 

I was using this cable since i had a cable which is used to connect cisco switches to com port. 

Let me try with USB-to-Serial Comm Port. 

I have another question. How to burn latest QorQ SDK to the SD card or internal storage in LS2088A RDB? 

what is the internal storage capacity which come along with package? 

Thanks,
Karthi 

0 Kudos
Reply

3,369 Views
ufedor
NXP Employee
NXP Employee

> I have another question. How to burn latest QorQ SDK to the SD card

> or internal storage in LS2088A RDB?

Please create new Community question for this request.

> what is the internal storage capacity which come along with package?

 The board has:

SPI flash

- MT25QU512ABB8ESF-0SIT (64 MB)

- S25FS512SAGNFI011 (64MB)

NOR flash
S29GL01GS11TFIV10 (128 MB)

NAND flash
MT29F16G08ABACAWP-Z:C (2 GB)

0 Kudos
Reply

3,369 Views
ufedor
NXP Employee
NXP Employee

> DB9 to RJ45 cable

This is a cable for the serial communication port (console).

> other way to connect to this Board other than CW

If you mean debugger connection, then a debugger is needed - for example Lauterbach.

1) The board comes with pre-installed firmware images produced by means of NXP LSDK - i.e. it is fully operational.

2) No.

0 Kudos
Reply