How to connect ls2088a using Console Cable DB9 to RJ45

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect ls2088a using Console Cable DB9 to RJ45

3,589 次查看
karthimohanraj_
Contributor I

I have to boot the LS2088A-RDB and i have a  DB9 to RJ45 cable. Will this be helpful in connecting since i don't have Codewarrior connector Or please suggest me any other way to connect to this Board other than CW.  

I have some queries regarding the LS2088A: 

1.  Does this board comes with all pre-installed BSP and SDK? so just connecting using DB9 cable should work out of the box? 

2. Is there any prerequisite settings and changes we should do in the LS2088A to use in the First boot.

Thanks,
karthi 

0 项奖励
回复
5 回复数

3,438 次查看
karthimohanraj_
Contributor I

Hi ufedor, 

I have tired connect with pci serial port adaptor(link) and DB9 to RJ45. But i'm not able to connect to Serial console, to check whether the LS2088A is booting or not. 

Can you point me to some connector available which works with LS2088A?

Thanks,
Karthi 

0 项奖励
回复

3,438 次查看
ufedor
NXP Employee
NXP Employee

Personally I'm using Prolific USB-to-Serial Comm Port.


Where did you get the DB9 to RJ45 cable?

The LS2088ARDB has standard DB9 connectors - no need in such cable:

2018-10-18_234450.jpg

0 项奖励
回复

3,438 次查看
karthimohanraj_
Contributor I

Hi Ufedor, 

I was using this cable since i had a cable which is used to connect cisco switches to com port. 

Let me try with USB-to-Serial Comm Port. 

I have another question. How to burn latest QorQ SDK to the SD card or internal storage in LS2088A RDB? 

what is the internal storage capacity which come along with package? 

Thanks,
Karthi 

0 项奖励
回复

3,438 次查看
ufedor
NXP Employee
NXP Employee

> I have another question. How to burn latest QorQ SDK to the SD card

> or internal storage in LS2088A RDB?

Please create new Community question for this request.

> what is the internal storage capacity which come along with package?

 The board has:

SPI flash

- MT25QU512ABB8ESF-0SIT (64 MB)

- S25FS512SAGNFI011 (64MB)

NOR flash
S29GL01GS11TFIV10 (128 MB)

NAND flash
MT29F16G08ABACAWP-Z:C (2 GB)

0 项奖励
回复

3,438 次查看
ufedor
NXP Employee
NXP Employee

> DB9 to RJ45 cable

This is a cable for the serial communication port (console).

> other way to connect to this Board other than CW

If you mean debugger connection, then a debugger is needed - for example Lauterbach.

1) The board comes with pre-installed firmware images produced by means of NXP LSDK - i.e. it is fully operational.

2) No.

0 项奖励
回复