How to add packages in systembuilder?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add packages in systembuilder?

Jump to solution
2,308 Views
adeel
Contributor III

Hello,

I want to add taskset command in the Systembuilder distribution. I tried opkg install taskset* but it doesn't work. Can anybody provide a link for Systembuilder package repository?

Adeel

1 Solution
1,745 Views
lunminliang
NXP Employee
NXP Employee

Please see below application team comment on this:

*******************************************************************

I believe the command is included as part of the util-linux package. (source: http://en.wikipedia.org/wiki/Util-linux) I have checked the Yocto packages with "bitbake -s" command and it appears to be present. Including the package with the build should give the command.

*******************************************************************

If possible you should upgrade the newest yocto SDK

View solution in original post

1 Reply
1,746 Views
lunminliang
NXP Employee
NXP Employee

Please see below application team comment on this:

*******************************************************************

I believe the command is included as part of the util-linux package. (source: http://en.wikipedia.org/wiki/Util-linux) I have checked the Yocto packages with "bitbake -s" command and it appears to be present. Including the package with the build should give the command.

*******************************************************************

If possible you should upgrade the newest yocto SDK