The memory dump of the GIC for the Grouping registers is
01410080: 00000000 00000000 00000000 00000000 ................
01410090: 00000000 00000000 00000000 00000000 ................
014100a0: 00000000 00000000 00000000 00000000 ................
014100b0: 00000000 00000000 00000000 00000000 ................
014100c0: 00000000 00000000 00000000 00000000 ................
014100d0: 00000000 00000000 00000000 00000000 ................
014100e0: 00000000 00000000 00000000 00000000 ................
014100f0: 00000000 00000000 00000000 00000000 ................
This means that all the interrupts are group 0? If all of them are group 0 [it is all 0 be default], i can not set the priority of the registers to non zero, and I would never get an interrupt as long as I am not in secure world [EL3] right?