Flash Address Selection for Lauterbach

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash Address Selection for Lauterbach

跳至解决方案
7,813 次查看
vinothkumars
Senior Contributor IV

Hi all,

I am using Lauterbach trace32 debugger with T4240RDB for flashing. I want to flash u-boot-spl.bin using sram.

I have the doubt in flash bass address. For lauterbach script which address want to use.

From QORIQ-SDK-2.0-IC-REV0.pdf

4.4.20.6 System Memory Map

0xfe0000000 - 0xfe7ffffff -  IFC - NOR Flash

4.4.20.7 Flash Bank Usage

0xE8000000 - 0xEFFFFFFF 

Thanks, VinothS

Regards,
Vinothkumar Sekar
0 项奖励
回复
1 解答
7,368 次查看
vinothkumars
Senior Contributor IV

Hi Matthias,

Thank you for reply.

My board have ddr controller issue. So, now I am using sram flash.

I generate u-boot-spl.bin (163.8KB) for u-boot debugging purpose and I check this map address (EFF40000) from u-boot-spl.map  and I flash this binary into same memory location 0xEFF40000 - 0xEFFFFFFF.

Flash was done properly. Now, I start u-boot debugging. 

If it possible please provide fix for this thread,

Lauterbach Trace32 Debugger with T4160RDB-64b 

https://community.nxp.com/thread/494768 

Regards, VinothS

Regards,
Vinothkumar Sekar

在原帖中查看解决方案

0 项奖励
回复
6 回复数
7,368 次查看
MatthiasB
Contributor II

Hello VinothS,

use the script in <your installation directory>\demo\powerpc64bit\hardware\qoriq_t4\all_boards\flash_cfi.cmm to prepare the flash process.
Answer the dialog "program now" with no and you will see the memory map of the flash in the Flash.List window.
You will see your 128MB flash, starting at F8000000 and ending at the end of the 32bit address range.
As your PC will start at 0xFFFFFFFC you have to flash your u-boot binary at the end of this 32bit address range.
The size of u-boot is 512KB, which means your starting address to flash this binary will be 0xFFF80000.

Use "FLASH.ReProgram ALL" to activate flash programming with check of sectors, then
Data.LOAD.Binary <path to u-boot binary> 0xFFF80000
You will then see changing sectors as "pending now" in the Flash.List window.
Using another "FLASH.ReProgram" command afterwards, the "pending" sectors will be flashed.

For more questions about the debugger, please contact us directly via [email protected]

Best regards,
Matthias

0 项奖励
回复
7,368 次查看
vinothkumars
Senior Contributor IV

Hi Matthias,

Thank you for your reply. 

https://community.nxp.com/message/807635?commentID=807635#comment-807635  

And I am following this thread according to this I configured NOR Flash device connected to CS0  as 0xE8000000

If it possible please provide the default location of RCW for Flash (or) please check my thread,

How to flash RCW binary/ Hard-coded RCW using lauterbach 

Regards, VinothS

Regards,
Vinothkumar Sekar
0 项奖励
回复
7,368 次查看
MatthiasB
Contributor II

Hi VinothS,

please follow my descriptions, it's just another address mapping in the script.

The NOR will be mapped to end of 32bit address range minus flash size (see inside).

The RCW is in the starting sector of the flash, in this case at 0xF8000000.

It won't work if you access non mapped address ranges as described in your other threads (0xE8yyyyyy).

Regards,

Matthias

0 项奖励
回复
7,368 次查看
vinothkumars
Senior Contributor IV

Hi Matthias,

Thank you for your reply.

I am using fresh board and I want to flash and boot u-boot alone.

In my case If NOR flash base address is 0xE8000000

As per document (https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf) for U-boot,

For RCW -> 0xE8000000

and U-boot -> 0XEFF40000

Is it wright ?

Regards,

VinothS 

Regards,
Vinothkumar Sekar
0 项奖励
回复
7,368 次查看
MatthiasB
Contributor II

Hi VinothS,

as you can read in your linked document, the bootloader even maps the NOR Flash to 0xFE8000000..

We us the same method in our flash_cfi.cmm scripts to map it to 0xF8000000.

Please read the chapter "Integrated Flash Controller (IFC)" in your processor reference manual to get an idea how it works and / or simply follow the description above (https://community.nxp.com/message/1108357?commentID=1108357&et=watches.email.thread#comment-1102911) to flash your u-boot binary. If you u-boot is 768KB as described you flash it to 0xFFF40000.

Regards,

Matthias

0 项奖励
回复
7,369 次查看
vinothkumars
Senior Contributor IV

Hi Matthias,

Thank you for reply.

My board have ddr controller issue. So, now I am using sram flash.

I generate u-boot-spl.bin (163.8KB) for u-boot debugging purpose and I check this map address (EFF40000) from u-boot-spl.map  and I flash this binary into same memory location 0xEFF40000 - 0xEFFFFFFF.

Flash was done properly. Now, I start u-boot debugging. 

If it possible please provide fix for this thread,

Lauterbach Trace32 Debugger with T4160RDB-64b 

https://community.nxp.com/thread/494768 

Regards, VinothS

Regards,
Vinothkumar Sekar
0 项奖励
回复