Ethernet header compression on QoriQ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ethernet header compression on QoriQ

1,362 次查看
viktarpalstsiuk
Contributor II

Are the any advised solutions for Ethernet header compression on QoriQ T1040 platform?

3 回复数

1,154 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Viktar,

Packet Data Convergence Protocol (abbrev. PDCP) is one of the layers of the Radio

Traffic Stack in UMTS and performs IP header compression and decompression, T1040 integrates SEC 5.4 supporting LTE PDCP.

IP Header Compression could be implemented over PPP, FMAN controller parser could support PPPoE+PPP.

If further discussion is needed, please describe your scenario in details.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,154 次查看
viktarpalstsiuk
Contributor II

We need to compress Ethernet header (SA+DA) in ethernet frame to send over custom 1Gb radio link. So we need to get Ethernet frame comming out of QoriQ with 2 or more bytes instead of full 12byte Ethetnet header. Is it possible?

0 项奖励
回复

1,154 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Viktar,

I think you could consider about PDCP solution mentioned previously, SDK 1.6 USDPAA contains an sample application "pdcp" in apps/simple_proto/app/, you could have a reference.

PDCP contains Ethernet header compression and ciphering(security), for security T1040 SEC component could provide support.

For PDCP Ethernet header compression, ROHC(Robust Header Compression) protocol is often used, please refer to the third party software http://cache.freescale.com/files/32bit/doc/white_paper/HDRCMPWP.pdf.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------