Hi,
I just wanted to create a profiling configuration for the t2080rb system.
Unfortunately I can't configure a connection for T2080, it's not listed in the dropdown menu. Just T4240, T4216 ...
Is profiling and tracing already available for the T2080 ?
I tried with CodeWarrior_PA_10.3.3 under Linux.
thanx and regards
Alois
Solved! Go to Solution.
T2080 is new devices supported in v10.4, that's why you can not see it in v10.3.3, the information could also be found in release note of 10.4.
So please update the tool from the link as Catalin provided above.
T2080 is new devices supported in v10.4, that's why you can not see it in v10.3.3, the information could also be found in release note of 10.4.
So please update the tool from the link as Catalin provided above.
I updated to v10.4.0.
T2080 profiling works perfect now.
thanxs and regards
Alois
hi,
You can find at this link
CodeWarrior Development Studio v10 for Power |Freescale
what devices are supported in Code Warrior and what is supported for each device.
You can find performance analysis supported for T2080 in Code Warrior 10.4.
regards,
Catalin