Dose the LS1043A support AVB protocol?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dose the LS1043A support AVB protocol?

2,268件の閲覧回数
d-z-c
Contributor III

Hi,sir.

We need to control and forward the AVB devices' streams by the LS1043A platform.

so I just wonder that how can LS1043A support AVB protocol if we don't link any switch.

Cause I have know tha the IMX6 or IMX8 support the AVB functions.

Dose the LS1043A chip have hardwate TIME_STAMP to support 802.1AS ?

And If AVB is supported to LS1043A,Then What we should do about the reference Software, kernel and rootfs and so on.

Kind Wishes.

GATSBY.

Have a good day.
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,178件の閲覧回数
ufedor
NXP Employee
NXP Employee

LS1043A does not support AVB as complete family of specificatons.

> Dose the LS1043A chip have hardwate TIME_STAMP to support 802.1AS ?

Yes, it has.

0 件の賞賛
返信

2,178件の閲覧回数
d-z-c
Contributor III

Hi ufedor, Why LS1043A not support AVB protocol? Is this a software(kernel,rootfs etc.) problem or a hardware problem?

Have a good day.
0 件の賞賛
返信

2,178件の閲覧回数
ufedor
NXP Employee
NXP Employee

Because of hardware limitations.

0 件の賞賛
返信