LS1046ARDB: First slot cannot be empty. ERROR: Parsing DIMM Error ERROR: DDR init failed. NOTICE: Incorrect DRAM0 size is defined in platfor_def.h ERROR: mmap_add_region_check() failed. er

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046ARDB: First slot cannot be empty. ERROR: Parsing DIMM Error ERROR: DDR init failed. NOTICE: Incorrect DRAM0 size is defined in platfor_def.h ERROR: mmap_add_region_check() failed. er

2,105 次查看
yuanqh
Contributor I

求助:

我在参考LS1046ARDB设计自己的板卡,没有使用CPLD,使用了内存颗粒芯片(MT40A512M16),uboot时打印如下信息:

First slot cannot be empty.
ERROR:   Parsing DIMM Error
ERROR:   DDR init failed.
NOTICE:  Incorrect DRAM0 size is defined in platfor_def.h
ERROR:   mmap_add_region_check() failed. error -22
ERROR:   mmap_add_region_check() failed. error -22
NOTICE:  BL2: v1.5(release):LSDK-19.09
NOTICE:  BL2: Built : 15:02:43, Apr 22 2020

0 项奖励
回复
1 回复

2,046 次查看
ufedor
NXP Employee
NXP Employee

Please describe the problem.

Is the RDB board factory-new?

0 项奖励
回复