Dose the LS1043A support AVB protocol?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dose the LS1043A support AVB protocol?

2,298 次查看
d-z-c
Contributor III

Hi,sir.

We need to control and forward the AVB devices' streams by the LS1043A platform.

so I just wonder that how can LS1043A support AVB protocol if we don't link any switch.

Cause I have know tha the IMX6 or IMX8 support the AVB functions.

Dose the LS1043A chip have hardwate TIME_STAMP to support 802.1AS ?

And If AVB is supported to LS1043A,Then What we should do about the reference Software, kernel and rootfs and so on.

Kind Wishes.

GATSBY.

Have a good day.
标记 (2)
0 项奖励
回复
3 回复数

2,208 次查看
ufedor
NXP Employee
NXP Employee

LS1043A does not support AVB as complete family of specificatons.

> Dose the LS1043A chip have hardwate TIME_STAMP to support 802.1AS ?

Yes, it has.

0 项奖励
回复

2,208 次查看
d-z-c
Contributor III

Hi ufedor, Why LS1043A not support AVB protocol? Is this a software(kernel,rootfs etc.) problem or a hardware problem?

Have a good day.
0 项奖励
回复

2,208 次查看
ufedor
NXP Employee
NXP Employee

Because of hardware limitations.

0 项奖励
回复