Difference between Active Debug Context and Project-specified debug contest in Codewarrior Flash Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between Active Debug Context and Project-specified debug contest in Codewarrior Flash Programmer

Jump to solution
4,662 Views
vinothkumars
Senior Contributor IV

Hi All,

I am using Codewarrior Flashprogrammer  version 10.7 for flash the images to T4160 Machine. After everything done, before execute I seen two type of Debug Context. Execute work after select the Projetc-specified debug context (Texst1_core00_RAM_T4160_Download).

I don know what is the difference and which one I want to use for flashing?  

Chosse Target Task file -> Change Run Configuration -> Select Run Configuration and Click -> ok in Target Task Pop Window.

pastedImage_1.png

If it possible, Please send to appropriate steps for flash by using Codewarrior Flashprogrammer version 10.7. Thank you for all! 

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
4,472 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply and Please Ignore this Thread.

Regards,

VinothS

Regards,
Vinothkumar Sekar

View solution in original post

0 Kudos
Reply
5 Replies
4,472 Views
vinothkumars
Senior Contributor IV

Hi All,

What are the configuration is must for flash using Codewarrior Flashprogrammer?

Please give some details and Thank you for all your support.

Thanks & Regards,

VinothS 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
4,472 Views
ufedor
NXP Employee
NXP Employee

Active Debug Context (= active debug session) is:

<> debug connection was established and is active

and

<> processor initialization script was executed

During a project creation it is possible to check Debug Configurations "Connect", "Download", "Connect SRAM" and "Download SRAM" - each of them can establish debug session required for the Flash Programmer.

Latter two can be used if SDRAM operation is unstable.

0 Kudos
Reply
4,467 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply.

I got some error while flashing and I tried the online solutions also. But, still I got the error by using Codewarrior Flashprogrammer. 

I set unprotect in action but, I got error protect/unprotect not support and why I am setting this because of Protection Sector Error.  

And also I attached the error log and flash programmer pdf document for your reference. Thanks for your support.


Error: Erase failed. Flash driver reports the following error(s): Sector Protection Error
Error: Erase failed. Flash driver reports the following error(s): Sector Protection Error

Error: Protect/Unprotect not supported on this device.
Error: Protect/Unprotect not supported on this device.

Thanks & Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply
4,467 Views
ufedor
NXP Employee
NXP Employee

What is the "GL01GS10FHI_new" in the Flash Error.txt?

0 Kudos
Reply
4,473 Views
vinothkumars
Senior Contributor IV

Hi Ufedor,

Thank you for your reply and Please Ignore this Thread.

Regards,

VinothS

Regards,
Vinothkumar Sekar
0 Kudos
Reply