Development Kit for QN9021

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Development Kit for QN9021

1,575 Views
abhishekparikh
Contributor I

As there is development kit available for QN9020.(a highly extensible platform for application develo|NXP ) I won't able to find development kit for QN9021. On that kit it is mentioned that it is compatible with SWD and UART interfaces for debug which is same for QN9021 so can I use the same for QN9021?

Regards

Abhishek Parikh 

0 Kudos
Reply
1 Reply

1,284 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The NXP does not provide development kit for the QN9021. The QN9020DK is based on the QN9020 which has 48 pins, while the QN9021 has 32 pins. There is a difference between the GPIO for the QN9021 and the QN9020. But the QN9020DK also can be used for software development for the QN9021. The QN9020 has all GPIOs available on the QN9021.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply