FDT_ERR on T1040 RDB board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FDT_ERR on T1040 RDB board

1,285件の閲覧回数
prashanthkumarg
Contributor I

Hi,

I'm using T1040RDB board, I have configured u-boot for Ram disk deployment from flash, I have used the following the image files from "QorIQ SDK v1.6 PPC64E5500 Image" :

 

1. uImage--3.12-r0t1040rdb-20140612105956

2. uImage--3.12-r0-t1040rdb-20140612105956.dtb

3. fsl-image-core-t1040rdb-20140613030314.rootfs.ext2.gz

 

All the files above mentioned are pre-built images, I have downloaded it via Kermit protocol. Unfortunately I'm not able to boo the linux image successfully and I'm receiving the "FDT_ERR_BADOFFSET" error message. I have attached the boot prompt and u-boot parameters output, request you to please help me on this.

 

Best regards

Prashanth

Original Attachment has been moved to: u-boot_latest.txt.zip

Original Attachment has been moved to: linux_updated.txt.zip

0 件の賞賛
返信
0 返答(返信)