Development Kit for QN9021

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Development Kit for QN9021

1,592件の閲覧回数
abhishekparikh
Contributor I

As there is development kit available for QN9020.(a highly extensible platform for application develo|NXP ) I won't able to find development kit for QN9021. On that kit it is mentioned that it is compatible with SWD and UART interfaces for debug which is same for QN9021 so can I use the same for QN9021?

Regards

Abhishek Parikh 

0 件の賞賛
返信
1 返信

1,301件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The NXP does not provide development kit for the QN9021. The QN9020DK is based on the QN9020 which has 48 pins, while the QN9021 has 32 pins. There is a difference between the GPIO for the QN9021 and the QN9020. But the QN9020DK also can be used for software development for the QN9021. The QN9020 has all GPIOs available on the QN9021.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信