DDR3L Write Performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3L Write Performance

2,785件の閲覧回数
kojimiura
Contributor III

When executing the following command on U-BOOT The first time was 414msec and Please tell me why the second and subsequent times are so slow as 541 msec.

mw.w ffa00008 f; mw.l 01000000 0 4000000; mw.w ffa00008 0

 

(ffa00008 : At the tp terminal of the PLD connected to the IFC bus
I measure time with an oscilloscope.)

 

0 件の賞賛
返信
5 返答(返信)

2,753件の閲覧回数
kojimiura
Contributor III
I would like to know why there is a large difference in DDR write time (about 100msec) even though the purpose is the same mw command.
We are considering an application that processes within a fixed period of time (5msec), so this difference cannot be ignored.
0 件の賞賛
返信

2,755件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Would you please let me know your purpose to do this experiment?

For DDR performance, we suggest you use Linux application "LMBench" to do testing.

0 件の賞賛
返信

2,716件の閲覧回数
kojimiura
Contributor III
I run LMbench.
I'll attach the results.
however,
There is no value in the Memory Write item.
I run everything by default Settings.
I would appreciate it if you could tell me how to measure memory performance using LMbench.

 

0 件の賞賛
返信

2,696件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download QorIQ SDK 2.0 user manual from the following link.

https://support.nxp.com/s/case/5002p00002zp58BAAQ/community-ddr3lwrite-performance?language=en_US

Then refer to the section "12.1.4 LMBench" in this document.

0 件の賞賛
返信

2,679件の閲覧回数
kojimiura
Contributor III

Thank you.

0 件の賞賛
返信