DDR3L Write Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3L Write Performance

2,779 Views
kojimiura
Contributor III

When executing the following command on U-BOOT The first time was 414msec and Please tell me why the second and subsequent times are so slow as 541 msec.

mw.w ffa00008 f; mw.l 01000000 0 4000000; mw.w ffa00008 0

 

(ffa00008 : At the tp terminal of the PLD connected to the IFC bus
I measure time with an oscilloscope.)

 

0 Kudos
Reply
5 Replies

2,747 Views
kojimiura
Contributor III
I would like to know why there is a large difference in DDR write time (about 100msec) even though the purpose is the same mw command.
We are considering an application that processes within a fixed period of time (5msec), so this difference cannot be ignored.
0 Kudos
Reply

2,749 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please let me know your purpose to do this experiment?

For DDR performance, we suggest you use Linux application "LMBench" to do testing.

0 Kudos
Reply

2,710 Views
kojimiura
Contributor III
I run LMbench.
I'll attach the results.
however,
There is no value in the Memory Write item.
I run everything by default Settings.
I would appreciate it if you could tell me how to measure memory performance using LMbench.

 

0 Kudos
Reply

2,690 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please download QorIQ SDK 2.0 user manual from the following link.

https://support.nxp.com/s/case/5002p00002zp58BAAQ/community-ddr3lwrite-performance?language=en_US

Then refer to the section "12.1.4 LMBench" in this document.

0 Kudos
Reply

2,673 Views
kojimiura
Contributor III

Thank you.

0 Kudos
Reply