Custom Board, Custom RCW for T1042 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom Board, Custom RCW for T1042 processor

Jump to solution
4,360 Views
yusufalti4444
Contributor I

Hi everyone,

We are working on a T1042 based Custom board. We have some differences when compared with RDB. We removed swithes which inditaces boot from where (NOR,NAND,SD).

What procedure should we follow when creating new PBL/RCW to change boot location using latest Code Warrior Flash programmer and QorIQ Suite together ? Is there any guide documentation ?

We are also open for other ideas.

Regards.

0 Kudos
Reply
1 Solution
4,072 Views
ufedor
NXP Employee
NXP Employee

It is reasonable to read the "QCVS PBL Tool User Guide" (Freescale\CW_PA_v10.5.1\eclipse\ProcessorExpert\Help\PDF\PBL Tool - User Guide.pdf)

View solution in original post

0 Kudos
Reply
5 Replies
4,072 Views
ufedor
NXP Employee
NXP Employee

> We removed swithes which inditaces boot from where (NOR,NAND,SD).

Please provide the processor connection schematics for inspection.

> creating new PBL/RCW to change boot location

Which boot source is planned to be used - refer to the QorIQ T1040 Reference Manual, 4.6.4.1 Reset configuration word (RCW) source.

0 Kudos
Reply
4,072 Views
yusufalti4444
Contributor I

> Please provide the processor connection schematics for inspection.

I am afraid but sharing is not applicable for me.

> Which boot source is planned to be used - refer to the QorIQ T1040 Reference Manual, 4.6.4.1 Reset configuration word (RCW) source.

This should be what I'm looking for. I'll only do 16 bit NOR flash booting. Does Code Warrior QCVS - RCW project have config variables to change these variables to generate new PBL ?

Thanks.

0 Kudos
Reply
4,072 Views
ufedor
NXP Employee
NXP Employee

> Does Code Warrior QCVS - RCW project have config variables to change these variables to generate new PBL ?

Sorry, which "these variables"?

0 Kudos
Reply
4,072 Views
yusufalti4444
Contributor I

index.jpeg

I mean, If it's posssible with Code Warrior, which configuration property should I change in a QCVS - RCW project ?

0 Kudos
Reply
4,073 Views
ufedor
NXP Employee
NXP Employee

It is reasonable to read the "QCVS PBL Tool User Guide" (Freescale\CW_PA_v10.5.1\eclipse\ProcessorExpert\Help\PDF\PBL Tool - User Guide.pdf)

0 Kudos
Reply