Configuration Space Address in PCIe (LS1046 ARDB)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuration Space Address in PCIe (LS1046 ARDB)

ソリューションへジャンプ
3,717件の閲覧回数
iqrajaved
Contributor III

Hi, 

Kindly provide me information about the configuration space address (lower base address to write in iATU) in PCIe controller working as RC so that I can translate a target address to the PCI memory. 

Also, what are the Host Outbound Memory and I/O base addresses in PCI. 

Best,

Iqra Javed

ラベル(1)
1 解決策
3,342件の閲覧回数
ufedor
NXP Employee
NXP Employee
The addresses in question are not static and can be assigned according to the application needs.
It is possible to refer to the following presentation:

元の投稿で解決策を見る

2 返答(返信)
3,343件の閲覧回数
ufedor
NXP Employee
NXP Employee
The addresses in question are not static and can be assigned according to the application needs.
It is possible to refer to the following presentation:
2,579件の閲覧回数
TrinathK
Contributor III

Hi @ufedor ,

The link you mentioned is expired. Please provide new link.

0 件の賞賛
返信