Configuration Space Address in PCIe (LS1046 ARDB)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuration Space Address in PCIe (LS1046 ARDB)

Jump to solution
3,738 Views
iqrajaved
Contributor III

Hi, 

Kindly provide me information about the configuration space address (lower base address to write in iATU) in PCIe controller working as RC so that I can translate a target address to the PCI memory. 

Also, what are the Host Outbound Memory and I/O base addresses in PCI. 

Best,

Iqra Javed

Labels (1)
1 Solution
3,363 Views
ufedor
NXP Employee
NXP Employee
The addresses in question are not static and can be assigned according to the application needs.
It is possible to refer to the following presentation:

View solution in original post

2 Replies
3,364 Views
ufedor
NXP Employee
NXP Employee
The addresses in question are not static and can be assigned according to the application needs.
It is possible to refer to the following presentation:
2,600 Views
TrinathK
Contributor III

Hi @ufedor ,

The link you mentioned is expired. Please provide new link.

0 Kudos
Reply