CodeWarrior NAND flash issues on P1020RDB-PD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior NAND flash issues on P1020RDB-PD

1,842 Views
ericfornstedt
Contributor III

Hi,

We are trying to put an image file to the NAND flash of our P1020RDB-PD board through
CodeWarrior's Flash Programmer, but have run into som problems. If we simply import the provided Target Task called P1020RDB-PD_NAND_FLASH, and use a run configuration which is set as "Connect" with the predefined target configuration P1020RDB-PD_RAM, it cannot erase or program the device with an "Erase and Program" operation.

Everything look alright to me until it all of a sudden just bail out with an error.

fl::target -lc "P1020RDB-PD RAM Connect"
fl::target -b 0x2000 0x30000
fl::target -v off -l on
cmdwin::fl::device -d "MT29F1G08ABAEA-eLBC" -o "128Mx8x1" -a 0x0 0x7ffffff
cmdwin::fl::image -f "/<very-long-path>/example.img" -t "Auto Detect" -re on -r 0x0 0x7ffffff -oe on -o 0x0
cmdwin::fl::erase image
 Beginning Operation ... 
------------------------- 
 log: Trying auto-detect... 
 log: File is NOT of type Elf Format. 
 log: File is NOT of type Motorola S-Record Format. 
Auto-detection is successful. 
 File is of type Binary/Raw Format. 
 
 log: Using Algorithm: MT29FxG08-eLBC.elf 
 log: 
 log: 
 log: ====================================================================== 
 log: === Target Configuration Settings 
 log: === Launch Configuration: P1020RDB-PD RAM Connect 
 log: ====================================================================== 
 log: Connecting ... 
Performing target initialization ... 
 log: Connected ... 
 log: 
 log: ====================================================================== 
 log: === Execute: Erase 
 log: === Timestamp: Tue Apr 25 14:00:27 2017 
 log: === Flash Device: MT29F1G08ABAEA-eLBC 
 log: === Flash Organization: 128Mx8x1 
 log: === Flash Mem Start Addr: 0x00000000 
 log: === Flash Mem End Addr: 0x07FFFFFF 
 log: ====================================================================== 
 Downloading Flash Device Driver ... 
 log: Loading Flash Device Driver at: 0x00002000 
 log: Flash Driver Buffer is at: 0x00008800 
 log: Flash Driver Buffer Size is: 0x00029800 
 log: 
 log: Writing the Address 
 log: Writing the address of the sector list 
 log: Clearing the status 
 log: Setting up Registers 
 log: Commanding target to run 
 Reading flash ID ...
 log: Reading init return status 
 log: Done 
 log: 
 log: Initialization Command Succeeded 
 log: Writing Erase Function Code 
 log: Writing the Address 
 log: Writing the Number of Sectors 
 log: Writing the address of the sector list 
 log: Writing the sector list 
Erasing Sector 0x00000000 to 0x0001FFFF 
 log: Clearing the status 
 log: Setting up Registers 
 log: Commanding target to run 
 Erasing ...
 log: Reading erase return status 
 Did not erase bad block at address 0x00000000 
Error: Erase failed.
 log: Timestamp: Tue Apr 25 14:00:32 2017 
Error: Erase failed.

What is more strange is that if I for example run a "Dump Flash" operation prior to the "Erase and Program" operation, the erase succeed, but it fails on the program step.

<---- Cut away identical log ------>
Erasing Sector 0x00000000 to 0x0001FFFF 
 log: Clearing the status 
 log: Setting up Registers 
 log: Commanding target to run 
 Erasing ...
 log: Reading erase return status 
 log: Done 
 Erase Command Succeeded 
 log: Timestamp: Tue Apr 25 14:24:32 2017 
cmdwin::fl::write
------------------------- 
Using restricted address range 0x00000000 to 0x07FFFFFF 
Programming file /<very-long-path>/example.img 
 log: Trying auto-detect... 
 log: File is NOT of type Elf Format. 
 log: File is NOT of type Motorola S-Record Format. 
Auto-detection is successful. 
 File is of type Binary/Raw Format. 
 
 log: Using Algorithm: MT29FxG08-eLBC.elf 
 log: 
 log: ====================================================================== 
 log: === Execute: Program 
 log: === Timestamp: Tue Apr 25 14:24:32 2017 
 log: === Flash Device: MT29F1G08ABAEA-eLBC 
 log: === Flash Organization: 128Mx8x1 
 log: === Flash Mem Start Addr: 0x00000000 
 log: === Flash Mem End Addr: 0x07FFFFFF 
 log: ====================================================================== 
 Downloading Flash Device Driver ... 
 log: Loading Flash Device Driver at: 0x00002000 
 log: Flash Driver Buffer is at: 0x00008800 
 log: Flash Driver Buffer Size is: 0x00029800 
 log: 
 log: Writing the Address 
 log: Writing the address of the sector list 
 log: Clearing the status 
 log: Setting up Registers 
 log: Commanding target to run 
 Reading flash ID ...
 log: Reading init return status 
 log: Done 
 log: 
 log: Initialization Command Succeeded 
 log: Trying auto-detect... 
 log: File is NOT of type Elf Format. 
 log: File is NOT of type Motorola S-Record Format. 
Auto-detection is successful. 
 File is of type Binary/Raw Format. 
 
Downloading 0x00010000 bytes to be programmed at 0x00000000 
Downloading 0x0000545C bytes to be programmed at 0x00010000 
 log: Programming 0x0000545C bytes of Target Memory at 0x00000000 
 log: Writing Program Function Code 
 log: Writing the Address 
 log: Writing the Size 
 log: Writing the address of the buffer 
 log: Clearing the status 
 log: Setting up Registers 
 log: Commanding target to run 
Executing program .... 
 log: Reading program return status 
Error: Program failed. Flash driver reports the following error(s): Bad block detected in flash at address 0x27051956
Error: Program failed. Flash driver reports the following error(s): Bad block detected in flash at address 0x27051956

Reading and writing NAND flash from within uBoot works fine, and if I examine the results of CodeWarrior's flash attempts I see that it can indeed erase the flash. It can also write something, but the data is corrupt somehow and is not the expected image file.

I also made a quick attempt to disable the bad block handling as suggested in another thread. The programming part did succeed then according to CodeWarrior log, but data was still corrupted on target so I guess that is not the way forward.

Does anyone have an idea of why we see these issues?

BR
/ Eric

0 Kudos
Reply
2 Replies

1,657 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Eric Fornstedt ,

I suggest you setup NOR Flash u-boot first, then mark the NAND flash block at address 0x27051956 as bad block under u-boot, please try u-boot command "nand markbad".

Thanks,

Yiping

0 Kudos
Reply

1,657 Views
ericfornstedt
Contributor III

Hello Yiping,

NOR Flash u-boot is already in place, and from there it is possible to flash NAND normally without issues. It is only from CodeWarrior it does not work.

I don't really see how marking address 0x27051956 as a bad block would be possible (I did try anyway, just in case). The P1020RDB-PD board has 128 MB of NAND flash only, so highest address would be 0x07FFFFFF right? And, the specific address/number 0x27051956 seems to be related to some magic number used by u-boot when I google it.

BR

/ Eric

0 Kudos
Reply