Card lockup problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Card lockup problem

1,659件の閲覧回数
zwg132883
Contributor III

Hi,

We are using T1042 CPU on our board. And package is built from yocto with follow meta-freescale commit id. linux kernel version is 4.14. 

we met an card reboot issue in field. The reboot reason is external watchdog. we have a process to fed the external watchdog periodically. Looks CPU was lockup/idle at that time so that cannot fed the watchdog.

Do you have any suggestion or debug method for this issue? thanks.

# sumo
meta-freescale 407c6cf408969445031a492e2d25e0e2749582ea

Kernel configuration is attached.

 

0 件の賞賛
返信
1 返信

1,656件の閲覧回数
ufedor
NXP Employee
NXP Employee

Possible points to check are:

1) ensure that the processor is not overheated

2) using CodeWarrior QCVS DDR Tool verify that DDR controller settings are optimal

3) whether external ESD events are possible?

4) if it is a single board failure - look for manufacturing defects

Further detailed investigation is possible if the issue can be replicated in the lab.

0 件の賞賛
返信