Can't setup profiling for T2080RDB ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't setup profiling for T2080RDB ?

Jump to solution
1,533 Views
aloishahn
Contributor III

Hi,

I just wanted to create a profiling configuration for the t2080rb system.

Unfortunately I can't configure a connection for T2080, it's not listed in the dropdown menu. Just T4240, T4216 ...

Is profiling and tracing already available for the T2080 ?

I tried with CodeWarrior_PA_10.3.3 under Linux.

thanx and regards

Alois

0 Kudos
Reply
1 Solution
1,386 Views
lunminliang
NXP Employee
NXP Employee

T2080 is new devices supported in v10.4, that's why you can not see it in v10.3.3, the information could also be found in release note of 10.4.

So please update the tool from the link as Catalin provided above.

View solution in original post

0 Kudos
Reply
3 Replies
1,387 Views
lunminliang
NXP Employee
NXP Employee

T2080 is new devices supported in v10.4, that's why you can not see it in v10.3.3, the information could also be found in release note of 10.4.

So please update the tool from the link as Catalin provided above.

0 Kudos
Reply
1,386 Views
aloishahn
Contributor III

I updated to v10.4.0.

T2080 profiling works perfect now.

thanxs and regards

Alois

0 Kudos
Reply
1,386 Views
catalindemergia
Contributor IV

hi,

You can find at this link

CodeWarrior Development Studio v10 for Power |Freescale

what devices are supported in Code Warrior and what is supported for each device.

You can find performance analysis supported for T2080 in Code Warrior 10.4.

regards,

Catalin