Can't setup profiling for T2080RDB ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't setup profiling for T2080RDB ?

ソリューションへジャンプ
2,633件の閲覧回数
aloishahn
Contributor III

Hi,

I just wanted to create a profiling configuration for the t2080rb system.

Unfortunately I can't configure a connection for T2080, it's not listed in the dropdown menu. Just T4240, T4216 ...

Is profiling and tracing already available for the T2080 ?

I tried with CodeWarrior_PA_10.3.3 under Linux.

thanx and regards

Alois

タグ(4)
0 件の賞賛
返信
1 解決策
2,486件の閲覧回数
lunminliang
NXP Employee
NXP Employee

T2080 is new devices supported in v10.4, that's why you can not see it in v10.3.3, the information could also be found in release note of 10.4.

So please update the tool from the link as Catalin provided above.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,487件の閲覧回数
lunminliang
NXP Employee
NXP Employee

T2080 is new devices supported in v10.4, that's why you can not see it in v10.3.3, the information could also be found in release note of 10.4.

So please update the tool from the link as Catalin provided above.

0 件の賞賛
返信
2,486件の閲覧回数
aloishahn
Contributor III

I updated to v10.4.0.

T2080 profiling works perfect now.

thanxs and regards

Alois

0 件の賞賛
返信
2,486件の閲覧回数
catalindemergia
Contributor IV

hi,

You can find at this link

CodeWarrior Development Studio v10 for Power |Freescale

what devices are supported in Code Warrior and what is supported for each device.

You can find performance analysis supported for T2080 in Code Warrior 10.4.

regards,

Catalin