Can't find apptrk in rootfs of fsl-image-core

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't find apptrk in rootfs of fsl-image-core

跳至解决方案
1,323 次查看
aloishahn
Contributor III

Hi,

I can't find the apptrk executable on my target, it should be at /usr/bin/apptrk, right ?

Should apptrk be included on the default system on the flash?

I also rebuilt the rootfs of  e.g.  fsl-image-core with same result.

I run a t2080rdb.

thanks

Alois

0 项奖励
回复
1 解答
1,179 次查看
aloishahn
Contributor III

Hi,

in the meantime I changed PRIVATE_FULL option to YES in the fsl-image-core recipe.

Seems to fix it, apptrk is included now.


PRIVATE_FULL = "yes"

in SDK/QorIQ-SDK-V1.6-20140619-yocto/meta-fsl-networking/images/fsl-image-core.bb

Alois



在原帖中查看解决方案

0 项奖励
回复
1 回复
1,180 次查看
aloishahn
Contributor III

Hi,

in the meantime I changed PRIVATE_FULL option to YES in the fsl-image-core recipe.

Seems to fix it, apptrk is included now.


PRIVATE_FULL = "yes"

in SDK/QorIQ-SDK-V1.6-20140619-yocto/meta-fsl-networking/images/fsl-image-core.bb

Alois



0 项奖励
回复