Can't find apptrk in rootfs of fsl-image-core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't find apptrk in rootfs of fsl-image-core

Jump to solution
1,320 Views
aloishahn
Contributor III

Hi,

I can't find the apptrk executable on my target, it should be at /usr/bin/apptrk, right ?

Should apptrk be included on the default system on the flash?

I also rebuilt the rootfs of  e.g.  fsl-image-core with same result.

I run a t2080rdb.

thanks

Alois

0 Kudos
Reply
1 Solution
1,176 Views
aloishahn
Contributor III

Hi,

in the meantime I changed PRIVATE_FULL option to YES in the fsl-image-core recipe.

Seems to fix it, apptrk is included now.


PRIVATE_FULL = "yes"

in SDK/QorIQ-SDK-V1.6-20140619-yocto/meta-fsl-networking/images/fsl-image-core.bb

Alois



View solution in original post

0 Kudos
Reply
1 Reply
1,177 Views
aloishahn
Contributor III

Hi,

in the meantime I changed PRIVATE_FULL option to YES in the fsl-image-core recipe.

Seems to fix it, apptrk is included now.


PRIVATE_FULL = "yes"

in SDK/QorIQ-SDK-V1.6-20140619-yocto/meta-fsl-networking/images/fsl-image-core.bb

Alois



0 Kudos
Reply