CCI-400 configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCI-400 configuration

2,505 Views
vijaykumardesai
Contributor II

I am trying to configure the CCI-400 to enable cache coherency.

I have a FPGA writing data to DDR and I am reading it from CPU [A72] in LS1046A.

But the cache does not get updated after the FPGA writes data to it. But if I invalidate the cache inbetween, it works fine.

I see that I am not able to configure any registers of CCI-400 [probably they are secure only registers and uboot leaves me in EL2].

Is there anyway I can check if the CCI works fine and maintain cache coherency.

0 Kudos
Reply
2 Replies

2,333 Views
IonutV_Vicovan
NXP Employee
NXP Employee

Hi, 

Did you get any progress with your issue?

I may have a similar issue on another platform.

Regards,

Ionut

0 Kudos
Reply

2,334 Views
vijaykumardesai
Contributor II

Hi,

It was some time ago, so I actually had to check what I did.

In my case the CCI configuration was OK. I could also check it with U-boot which allowed me to enter in EL3. MMU configuration was also OK. The issue was in our test, I did not have a sync barrier between 'FPGA writing to memory' and 'CPU reading from memory'. So the instructions were executed out of order and read from memory was faster than write to FPGA. When I disabled cache, read from DDR was slow enough for FPGA to finish writing.

Sync barrier [both data and instruction] helped in my case.

It depends on what you actually want to do.

0 Kudos
Reply