strongswan

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

strongswan

2,211 次查看
2979338158
Contributor I

Hello, when I use NXP openwrt ls1012a to execute strongswan IPSec to build a tunnel, the kernel will report the following errors. Thank you very much for your help in analyzing them.

Error messages are in the vicinity !

标签 (1)
0 项奖励
回复
2 回复数

2,025 次查看
bpe
NXP Employee
NXP Employee

Consider using NXP ASK which is based on OpenWRT customized and verified
on LS1012A-based boards:

Layerscape 1012A Broadband Home Router Application | NXP 

The ASK offers an NXP verified and HW-accelerated IPSec solution.

Regards,

Platon

0 项奖励
回复

2,025 次查看
bpe
NXP Employee
NXP Employee

Can you please mention the exact name and version of the NXP SDK/BSP you are
working with?

Best Regards,

Platon

0 项奖励
回复