C29x in centos 6.5, when i build sdk , there are some problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C29x in centos 6.5, when i build sdk , there are some problems

1,049 Views
wujm
Contributor I

i want to use nginx and openssl to accelate ssl

choose p4080ds

bitbake fsl-image-core

Exception: CalledProcessError: Command 'cd /export/work/QorIQ-SDK-V2.0-20160527-yocto/build_p4080ds/tmp/work/x86_64-linux/quilt-native/0.64-r0/sysroot-destdir/export/work/QorIQ-SDK-V2.0-20160527-yocto/build_p4080ds/tmp/sysroots/x86_64-linux; find . -type d -print | tar -cf - -C /export/work/QorIQ-SDK-V2.0-20160527-yocto/build_p4080ds/tmp/work/x86_64-linux/quilt-native/0.64-r0/sysroot-destdir/export/work/QorIQ-SDK-V2.0-20160527-yocto/build_p4080ds/tmp/sysroots/x86_64-linux -p --files-from - --no-recursion | tar -xf - -C /export/work/QorIQ-SDK-V2.0-20160527-yocto/build_p4080ds/tmp/sysroots/x86_64-linux' returned non-zero exit status 2 with output tar: ./usr/bin: Cannot utime: No such file or directory
tar: ./usr/bin: Cannot stat: No such file or directory
tar: ./usr/share/quilt/scripts: Cannot utime: No such file or directory
tar: ./usr/share/quilt/scripts: Cannot stat: No such file or directory
tar: ./usr/share/quilt/compat: Cannot utime: No such file or directory
tar: ./usr/share/quilt/compat: Cannot stat: No such file or directory
tar: ./sysroot-providers: Cannot utime: No such file or directory
tar: ./sysroot-providers: Cannot stat: No such file or directory
tar: ./etc/bash_completion.d: Cannot utime: No such file or directory
tar: ./etc/bash_completion.d: Cannot stat: No such file or directory
tar: Exiting with failure status due to previous errors

0 Kudos
Reply
1 Reply

875 Views
cristians
NXP Employee
NXP Employee

Apparently the core image build for P4080 fails. It's an unusual error. Do you get the same error for other images or platforms?

0 Kudos
Reply