p1022 power on reset problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p1022 power on reset problem

727件の閲覧回数
zeevg
Contributor I

Hi,

I working to bring up new board.

I see problem booting from parallel nor.

When making the reset via the ICE the booting is started.

when booting after power up or using reset switch (connected to the input of supervisory) the booting sometime not started.

I drive The CPU HRESET pin from supervisory (which guaranty clean and long signal) to AND gate which inputs are the ICE_Hreset and POReset.

In addition AND gate which inputs are the ICE_TRST and POReset drive the CPU TRST pin.

Pls. advise

Zeev Gerber

0 件の賞賛
返信
1 返信

656件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is needed to check the processor connection schematics as a whole.

Please create a Technical Case and provide the schematics:

https://community.freescale.com/thread/381898

0 件の賞賛
返信