C29x PKCAL - RSVDx Pin Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

C29x PKCAL - RSVDx Pin Connection

ソリューションへジャンプ
1,848件の閲覧回数
samjackson
Contributor II

Hello - hope someone can help please.

Ref C29x in PKCAL mode, pins RSVD09..62 have Note #15:

"15. These pins must be pulled to ground (GND)."

This suggests these pins need to have pull-down resistor(s) to GND.

Is this a correct interpretation or is it acceptable to tie these pins directly to GND?
If pull-down resistors are needed - what value is suggested?

Reference Document used: C29x Crypto Coprocessor Family Data Sheet for PKCAL Mode, Rev0, Page 34.

Many thanks,

SJ

タグ(2)
1 解決策
1,800件の閲覧回数
ufedor
NXP Employee
NXP Employee

> is it acceptable to tie these pins directly to GND?

Yes.

元の投稿で解決策を見る

1 返信
1,801件の閲覧回数
ufedor
NXP Employee
NXP Employee

> is it acceptable to tie these pins directly to GND?

Yes.