Bank Selection Bits in DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bank Selection Bits in DDR3

970 Views
qammarabbas
Contributor IV

query.png

Hi,
The attached picture is taken from the reference manual of T1042. The query here is why there are only 2 sub-bank selection bits shown on each chip (indicated in red)? In this example all 8 sub banks are being used, and for that to happen we need 3 sub-bank selection bits (indicated in red in DDR controller). Please let me know where is the 3rd bit? Thank you!

Tags (1)
2 Replies

870 Views
ufedor
NXP Employee
NXP Employee

You are right - the picture has to be corrected.

You can refer to the T1040RDB design files available here:

QorIQ T1040 Reference Design Board|NXP 

870 Views
qammarabbas
Contributor IV

Thank you ufedor‌!
But i found this to be correct. The reason being in this diagram, each SDRAM device is of 64Mbits and according to the datasheet of 64Mbits SDRAM device it can only support 4 internal(logical) banks, therefore it will use only 2 bits instead of 3 for sub-bank selection.

0 Kudos
Reply