Bank Selection Bits in DDR3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bank Selection Bits in DDR3

971件の閲覧回数
qammarabbas
Contributor IV

query.png

Hi,
The attached picture is taken from the reference manual of T1042. The query here is why there are only 2 sub-bank selection bits shown on each chip (indicated in red)? In this example all 8 sub banks are being used, and for that to happen we need 3 sub-bank selection bits (indicated in red in DDR controller). Please let me know where is the 3rd bit? Thank you!

タグ(1)
2 返答(返信)

871件の閲覧回数
ufedor
NXP Employee
NXP Employee

You are right - the picture has to be corrected.

You can refer to the T1040RDB design files available here:

QorIQ T1040 Reference Design Board|NXP 

871件の閲覧回数
qammarabbas
Contributor IV

Thank you ufedor‌!
But i found this to be correct. The reason being in this diagram, each SDRAM device is of 64Mbits and according to the datasheet of 64Mbits SDRAM device it can only support 4 internal(logical) banks, therefore it will use only 2 bits instead of 3 for sub-bank selection.

0 件の賞賛
返信