B4860QDS DMA shows Transfer Error. That's it

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

B4860QDS DMA shows Transfer Error. That's it

Jump to solution
1,539 Views
mihaiciric
Contributor II

I am using the netcomm ocn dma api to transfer using simple mode mem2mem. I am getting a Transfer Error, but no other information on the cause.

Is there any needed pamu/liodn changes that need to be taken cared off for simple mem2mem? The reference manual is extremely vague!

Thanks,

Mihai

0 Kudos
Reply
1 Solution
1,423 Views
mihaiciric
Contributor II

I found the issue. Turns out I needed to use PAMU for mem2mem.

Thanks

View solution in original post

0 Kudos
Reply
2 Replies
1,424 Views
mihaiciric
Contributor II

I found the issue. Turns out I needed to use PAMU for mem2mem.

Thanks

0 Kudos
Reply
1,423 Views
alexander_yakov
NXP Employee
NXP Employee

Reference Manual states there is a number of number of possible reasons for transfer error - "non-correctable ECC errors on memory accesses, parity

errors on flash controller, address mapping errors, and so on". But, DMA controller itself does not offer more details, the only "Transfer Error" bit is available in SRn.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply