B4860QDS DMA shows Transfer Error. That's it

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

B4860QDS DMA shows Transfer Error. That's it

ソリューションへジャンプ
1,535件の閲覧回数
mihaiciric
Contributor II

I am using the netcomm ocn dma api to transfer using simple mode mem2mem. I am getting a Transfer Error, but no other information on the cause.

Is there any needed pamu/liodn changes that need to be taken cared off for simple mem2mem? The reference manual is extremely vague!

Thanks,

Mihai

0 件の賞賛
返信
1 解決策
1,419件の閲覧回数
mihaiciric
Contributor II

I found the issue. Turns out I needed to use PAMU for mem2mem.

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,420件の閲覧回数
mihaiciric
Contributor II

I found the issue. Turns out I needed to use PAMU for mem2mem.

Thanks

0 件の賞賛
返信
1,419件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Reference Manual states there is a number of number of possible reasons for transfer error - "non-correctable ECC errors on memory accesses, parity

errors on flash controller, address mapping errors, and so on". But, DMA controller itself does not offer more details, the only "Transfer Error" bit is available in SRn.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信