About aurora interface on T2080.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About aurora interface on T2080.

1,812件の閲覧回数
pilkyojeong
Contributor I

Hi, I have a question about aurora interface.

I'd like to know the pin map of aurora on T2080.

if anyone knows, please let me know.

Thanks.

タグ(2)
0 件の賞賛
返信
1 返信

1,669件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

The T2080 SERDES2 lanes E and F can be configured for the AURORA (see Table “SerDes Lanes Assignments and Multiplexing” in the T2080 reference manual available on the NXP site). Lane E signals are SD2_TX4_P/SD2_TX4_N and SD2_RX4_P/SD2_RX4_N. Lanes F signals are SD2_TX5_P/SD2_TX5_N and SD2_RX5_P/SD2_RX5_N (see Table “SerDes 2 Lane Assignments” in the T2080 reference manual). According to the T2080 data sheet these signals provides on the next package balls
SD2_TX4_N on AG5
SD2_TX4_P on AF5
SD2_RX4_N on AK5
SD2_RX4_P on AJ5
SD2_TX5_N on AF6
SD2_TX5_P on AG6
SD2_RX5_N on AJ6
SD2_RX5_P on AK6

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信