Have a great day,
The T2080 SERDES2 lanes E and F can be configured for the AURORA (see Table “SerDes Lanes Assignments and Multiplexing” in the T2080 reference manual available on the NXP site). Lane E signals are SD2_TX4_P/SD2_TX4_N and SD2_RX4_P/SD2_RX4_N. Lanes F signals are SD2_TX5_P/SD2_TX5_N and SD2_RX5_P/SD2_RX5_N (see Table “SerDes 2 Lane Assignments” in the T2080 reference manual). According to the T2080 data sheet these signals provides on the next package balls
SD2_TX4_N on AG5
SD2_TX4_P on AF5
SD2_RX4_N on AK5
SD2_RX4_P on AJ5
SD2_TX5_N on AF6
SD2_TX5_P on AG6
SD2_RX5_N on AJ6
SD2_RX5_P on AK6
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------