T1024 core architecture

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1024 core architecture

1,669 次查看
abineshselvaraj
Contributor III

Hi,

We are using T1024RDB for our project. It is understood that, T1024 integrates e5500 dual core architecture. Is this architecture is equal or compatible to PPC85XX or mpc855xx.

Thanks,

S.Abinesh.

0 项奖励
回复
1 回复

1,531 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

The e5500 provides the next-generation core technology available in the Freescale e500 family, enabling designers to take advantage of 64-bit processing through an optimized core well-suited for multicore environments. The e5500 core is software compatible with the rest of the e500 family. Designers have the option to run the core in 32-bit mode, making it a seamless migration from previous e500-based products.

See short review the e5500 Core in

http://cache.nxp.com/files/64bit/doc/white_paper/64BTTCHNLGYWP.pdf 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复