Is there any sample project to test TDM interface in PSC9131 Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any sample project to test TDM interface in PSC9131 Board

跳至解决方案
2,996 次查看
vinoths
Contributor I

Hi All,

How to test whether TDM interface is working in PSC9131 Board ?

Is there any sample or demo project to test it ?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,722 次查看
lunminliang
NXP Employee
NXP Employee

I am afraid The 9131TDM demo is not available.
You can use the SDOS TDM driver to create one. In case you have any issue with SDOS driver, pls file a new ticket on that.
The demo available in 815x can also be used as reference.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,722 次查看
andreiroman
Contributor I

I would like an answer to this question too.

I only found a loopback example in SDOS, but it does not help.

0 项奖励
回复
2,723 次查看
lunminliang
NXP Employee
NXP Employee

I am afraid The 9131TDM demo is not available.
You can use the SDOS TDM driver to create one. In case you have any issue with SDOS driver, pls file a new ticket on that.
The demo available in 815x can also be used as reference.

0 项奖励
回复