Is there any sample project to test TDM interface in PSC9131 Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any sample project to test TDM interface in PSC9131 Board

Jump to solution
2,452 Views
vinoths
Contributor I

Hi All,

How to test whether TDM interface is working in PSC9131 Board ?

Is there any sample or demo project to test it ?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,178 Views
lunminliang
NXP Employee
NXP Employee

I am afraid The 9131TDM demo is not available.
You can use the SDOS TDM driver to create one. In case you have any issue with SDOS driver, pls file a new ticket on that.
The demo available in 815x can also be used as reference.

View solution in original post

0 Kudos
Reply
2 Replies
2,178 Views
andreiroman
Contributor I

I would like an answer to this question too.

I only found a loopback example in SDOS, but it does not help.

0 Kudos
Reply
2,179 Views
lunminliang
NXP Employee
NXP Employee

I am afraid The 9131TDM demo is not available.
You can use the SDOS TDM driver to create one. In case you have any issue with SDOS driver, pls file a new ticket on that.
The demo available in 815x can also be used as reference.

0 Kudos
Reply