ADI scripts for 913x platforms Required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADI scripts for 913x platforms Required

5,687 Views
ambarish_a
Contributor I

We are using the 9132 QDS board with Benetel TDD RF. We are looking for the ADI script to be used for 10MHz. 

Can someone share the working ADI scripts?

Details:

RF version is Rev 1.4

9132QDS Board

TDD Mode

10MHz

L1 version used 2.1p3

We tried using the ones from 9131 FDD(Did the freq related changes for TDD) but we see below error.

fsl-aic ff650000.aic: rf0:sync did not clr 80000002
rf0: Failed start, err 11

0 Kudos
Reply
2 Replies

5,550 Views
ambarish_a
Contributor I

Did not see any attachment from your response. However, we got the ADI scripts from Benetel and it works. Thank you.

0 Kudos
Reply

5,550 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether the attached script is what you need.

0 Kudos
Reply