ADI scripts for 913x platforms Required

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADI scripts for 913x platforms Required

5,673件の閲覧回数
ambarish_a
Contributor I

We are using the 9132 QDS board with Benetel TDD RF. We are looking for the ADI script to be used for 10MHz. 

Can someone share the working ADI scripts?

Details:

RF version is Rev 1.4

9132QDS Board

TDD Mode

10MHz

L1 version used 2.1p3

We tried using the ones from 9131 FDD(Did the freq related changes for TDD) but we see below error.

fsl-aic ff650000.aic: rf0:sync did not clr 80000002
rf0: Failed start, err 11

0 件の賞賛
返信
2 返答(返信)

5,536件の閲覧回数
ambarish_a
Contributor I

Did not see any attachment from your response. However, we got the ADI scripts from Benetel and it works. Thank you.

0 件の賞賛
返信

5,536件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please check whether the attached script is what you need.

0 件の賞賛
返信