weak definitions of handlers in Events.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

weak definitions of handlers in Events.c

899 Views
mentair
Contributor I

Hello,

is it possible to cause the code generation process to generate __weak definitions of the event handlers in Events.c (in this case for the ARM Compiler)?  I reckon that one would have to modify the component "Events" with the Component Development Environment?  This behaviour would be useful because we use the generated ProcessorExpert Code as a library for several reasons.  Having weak referenes allows to overwrite the handlers one by one in ongoing development, and not being forced to provide stubs for newly generated components not yet in use.

Regards,

Martin

Tags (1)
0 Kudos
Reply
1 Reply

816 Views
vfilip
NXP Employee
NXP Employee

Hello,

this is not supported, however I have passed this to developers to consider it.

best regards

Vojtech Filip

Processor Expert Support Team


0 Kudos
Reply