weak definitions of handlers in Events.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

weak definitions of handlers in Events.c

946 次查看
mentair
Contributor I

Hello,

is it possible to cause the code generation process to generate __weak definitions of the event handlers in Events.c (in this case for the ARM Compiler)?  I reckon that one would have to modify the component "Events" with the Component Development Environment?  This behaviour would be useful because we use the generated ProcessorExpert Code as a library for several reasons.  Having weak referenes allows to overwrite the handlers one by one in ongoing development, and not being forced to provide stubs for newly generated components not yet in use.

Regards,

Martin

标记 (1)
0 项奖励
回复
1 回复

863 次查看
vfilip
NXP Employee
NXP Employee

Hello,

this is not supported, however I have passed this to developers to consider it.

best regards

Vojtech Filip

Processor Expert Support Team


0 项奖励
回复