weak definitions of handlers in Events.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

weak definitions of handlers in Events.c

881件の閲覧回数
mentair
Contributor I

Hello,

is it possible to cause the code generation process to generate __weak definitions of the event handlers in Events.c (in this case for the ARM Compiler)?  I reckon that one would have to modify the component "Events" with the Component Development Environment?  This behaviour would be useful because we use the generated ProcessorExpert Code as a library for several reasons.  Having weak referenes allows to overwrite the handlers one by one in ongoing development, and not being forced to provide stubs for newly generated components not yet in use.

Regards,

Martin

タグ(1)
0 件の賞賛
返信
1 返信

798件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

this is not supported, however I have passed this to developers to consider it.

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信