k60 USB0 settings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

k60 USB0 settings

跳至解决方案
2,133 次查看
bataliero
Contributor III

cpu

 

My cpu settings : I use PLL and 8MHz external crystal

but when I try to use USB - error occurs:

" No timing clock signal for device USB0 (FLL is disabled in the PEE MCG mode. See 'MCG settigns/FLL settings' of the 'Clock source setting 0' used by the 'Clock configuration 0' in cpu component.) "

 

 

How to turn USB  on?

 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,878 次查看
MVa
NXP Employee
NXP Employee

Hi,

  switch to the "Expert" view and  in the "Cpu" component select "PLL clock" value in the "PLL/FLL clock selection" property (see attached picture).

 

MVa

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,879 次查看
MVa
NXP Employee
NXP Employee

Hi,

  switch to the "Expert" view and  in the "Cpu" component select "PLL clock" value in the "PLL/FLL clock selection" property (see attached picture).

 

MVa

0 项奖励
回复