k60 USB0 settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

k60 USB0 settings

Jump to solution
2,224 Views
bataliero
Contributor II

cpu

 

My cpu settings : I use PLL and 8MHz external crystal

but when I try to use USB - error occurs:

" No timing clock signal for device USB0 (FLL is disabled in the PEE MCG mode. See 'MCG settigns/FLL settings' of the 'Clock source setting 0' used by the 'Clock configuration 0' in cpu component.) "

 

 

How to turn USB  on?

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,969 Views
MVa
NXP Employee
NXP Employee

Hi,

  switch to the "Expert" view and  in the "Cpu" component select "PLL clock" value in the "PLL/FLL clock selection" property (see attached picture).

 

MVa

View solution in original post

0 Kudos
Reply
1 Reply
1,970 Views
MVa
NXP Employee
NXP Employee

Hi,

  switch to the "Expert" view and  in the "Cpu" component select "PLL clock" value in the "PLL/FLL clock selection" property (see attached picture).

 

MVa

0 Kudos
Reply